ManikinBuilderSAEPercentileType Enumeration¶
NXOpen.Features.VehicleDesign.ManikinBuilder.SAEPercentileType is an alias for NXOpen.Features.VehicleDesign.ManikinBuilderSAEPercentileType
-
class
NXOpen.Features.VehicleDesign.
ManikinBuilderSAEPercentileType
¶ Bases:
object
the vehicle percentile type
Enum Members
Enum Member Enum Member Description J826Type95thPercentile 95th Percentile SAE j826 Standard Type J826Type50thPercentile 50th Percentile SAE j826 Standard Type J826Type10thPercentile 10th Percentile SAE j826 Standard Type J833LargeHuman95thMale Large Human SAE j833 Standard Type J833MediumHumanHalfwayPosition Medium Human SAE j833 Standard Type J833SmallHuman5thFemale Small Human SAE j833 Standard Type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-