InnerAngleBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
InnerAngleBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.InnerAngle
builder, used to create or edit inner angle feature.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateInnerAngleBuilder
Default values.
Property Value CalculationMethod Circular InnerAngle.Value 14 RequirementsControl StandardDriven ShowDistanceMeasurement 0 Visualization Curve WheelSize StaticRadius New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CalculationMethod | Returns or sets the calculation method type which determines the calculation method in the inner angle. |
CarBodyFaces | Returns the selected car body faces for measurement. |
InnerAngle | Returns the expression containing the inner angle. |
Loading | Returns or sets the loading used in the inner angle. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RequirementsControl | Returns or sets the requirements control for standard driven or user defined. |
ShowDistanceMeasurement | Returns or sets the value to show distance measurement. |
Standard | Returns or sets the standard used to define the inner angle. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Visualization | Returns or sets the visualization type of the inner angle output. |
WheelSize | Returns or sets the wheel size type which determines the size of the wheels in the inner angle. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InnerAngleBuilderCalculationMethodType Enumeration | Represents the calculation method types to calculate inner angle output. |
InnerAngleBuilderRequirementsControlType Enumeration | Represents the requirements control types to define the inner angle. |
InnerAngleBuilderVisualizationType Enumeration | Represents the visualization types of the output. |
InnerAngleBuilderWheelSizeType Enumeration | Represents the wheel size types to calculate inner angle output. |
Property Detail¶
CalculationMethod¶
-
InnerAngleBuilder.
CalculationMethod
¶ Returns or sets the calculation method type which determines the calculation method in the inner angle.
-------------------------------------
Getter Method
Signature
CalculationMethod()
Returns: Return type: NXOpen.Features.VehicleDesign.InnerAngleBuilderCalculationMethodType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CalculationMethod(calculationMethod)
Parameters: calculationMethod ( NXOpen.Features.VehicleDesign.InnerAngleBuilderCalculationMethodType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
CarBodyFaces¶
-
InnerAngleBuilder.
CarBodyFaces
¶ Returns the selected car body faces for measurement.
-------------------------------------
Getter Method
Signature
CarBodyFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
InnerAngle¶
-
InnerAngleBuilder.
InnerAngle
¶ Returns the expression containing the inner angle.
-------------------------------------
Getter Method
Signature
InnerAngle()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Loading¶
-
InnerAngleBuilder.
Loading
¶ Returns or sets the loading used in the inner angle.
-------------------------------------
Getter Method
Signature
Loading()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Loading(loading)
Parameters: loading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RequirementsControl¶
-
InnerAngleBuilder.
RequirementsControl
¶ Returns or sets the requirements control for standard driven or user defined.
-------------------------------------
Getter Method
Signature
RequirementsControl()
Returns: Return type: NXOpen.Features.VehicleDesign.InnerAngleBuilderRequirementsControlType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementsControl(requirementsControl)
Parameters: requirementsControl ( NXOpen.Features.VehicleDesign.InnerAngleBuilderRequirementsControlType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowDistanceMeasurement¶
-
InnerAngleBuilder.
ShowDistanceMeasurement
¶ Returns or sets the value to show distance measurement.
True will show the distance measurement. False will hide the distance measurement.
-------------------------------------
Getter Method
Signature
ShowDistanceMeasurement()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowDistanceMeasurement(showDistanceMeasurement)
Parameters: showDistanceMeasurement (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Standard¶
-
InnerAngleBuilder.
Standard
¶ Returns or sets the standard used to define the inner angle.
-------------------------------------
Getter Method
Signature
Standard()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard(standard)
Parameters: standard (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Visualization¶
-
InnerAngleBuilder.
Visualization
¶ Returns or sets the visualization type of the inner angle output.
See
NXOpen.Features.VehicleDesign.InnerAngleBuilderVisualizationType
for valid values.-------------------------------------
Getter Method
Signature
Visualization()
Returns: Return type: NXOpen.Features.VehicleDesign.InnerAngleBuilderVisualizationType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visualization(visualization)
Parameters: visualization ( NXOpen.Features.VehicleDesign.InnerAngleBuilderVisualizationType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
WheelSize¶
-
InnerAngleBuilder.
WheelSize
¶ Returns or sets the wheel size type which determines the size of the wheels in the inner angle.
-------------------------------------
Getter Method
Signature
WheelSize()
Returns: Return type: NXOpen.Features.VehicleDesign.InnerAngleBuilderWheelSizeType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WheelSize(wheelSize)
Parameters: wheelSize ( NXOpen.Features.VehicleDesign.InnerAngleBuilderWheelSizeType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
InnerAngleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.