BaseDataLoadingWheelBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
BaseDataLoadingWheelBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder
.This class can only be used in base data, thus cannot be created directly by user.
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Camber | Returns or sets the camber of wheel in degree. |
CoordinateX | Returns or sets the x coordinate of wheel center point. |
CoordinateY | Returns or sets the y coordinate of wheel center point. |
CoordinateZ | Returns or sets the z coordinate of wheel center point. |
DataDefinition | Returns or sets the value to indicate which definition option will be used to define the loading wheel data. |
DeltaCamber | Returns or sets the delta camber of wheel. |
DeltaStaticRadius | Returns or sets the delta static radius of wheel. |
DeltaToe | Returns or sets the delta toe of wheel. |
DeltaX | Returns or sets the delta x value of wheel center point. |
DeltaY | Returns or sets the delta y value of wheel center point. |
DeltaZ | Returns or sets the delta z value of wheel center point. |
DesignData | Returns or sets the design data of the wheel. |
StaticRadius | Returns or sets the static radius of wheel. |
Tag | Returns the Tag for this object. |
Toe | Returns or sets the toe in/out of wheel in degree. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BaseDataLoadingWheelBuilderDataDefinitionOptions Enumeration | This enum represents the options to define the wheel position. |
Property Detail¶
Camber¶
-
BaseDataLoadingWheelBuilder.
Camber
¶ Returns or sets the camber of wheel in degree.
Used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Absolute
.-------------------------------------
Getter Method
Signature
Camber()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Camber(camber)
Parameters: camber (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
CoordinateX¶
-
BaseDataLoadingWheelBuilder.
CoordinateX
¶ Returns or sets the x coordinate of wheel center point.
Used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Absolute
.-------------------------------------
Getter Method
Signature
CoordinateX()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateX(absX)
Parameters: absX (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
CoordinateY¶
-
BaseDataLoadingWheelBuilder.
CoordinateY
¶ Returns or sets the y coordinate of wheel center point.
Used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Absolute
.-------------------------------------
Getter Method
Signature
CoordinateY()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateY(absY)
Parameters: absY (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
CoordinateZ¶
-
BaseDataLoadingWheelBuilder.
CoordinateZ
¶ Returns or sets the z coordinate of wheel center point.
Used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Absolute
.-------------------------------------
Getter Method
Signature
CoordinateZ()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateZ(absZ)
Parameters: absZ (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DataDefinition¶
-
BaseDataLoadingWheelBuilder.
DataDefinition
¶ Returns or sets the value to indicate which definition option will be used to define the loading wheel data.
-------------------------------------
Getter Method
Signature
DataDefinition()
Returns: Return type: NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DataDefinition(dataDefinition)
Parameters: dataDefinition ( NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DeltaCamber¶
-
BaseDataLoadingWheelBuilder.
DeltaCamber
¶ Returns or sets the delta camber of wheel.
It is used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Relative
.-------------------------------------
Getter Method
Signature
DeltaCamber()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeltaCamber(deltaCamber)
Parameters: deltaCamber (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DeltaStaticRadius¶
-
BaseDataLoadingWheelBuilder.
DeltaStaticRadius
¶ Returns or sets the delta static radius of wheel.
It is used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Relative
.-------------------------------------
Getter Method
Signature
DeltaStaticRadius()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeltaStaticRadius(deltaStaticRadius)
Parameters: deltaStaticRadius (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DeltaToe¶
-
BaseDataLoadingWheelBuilder.
DeltaToe
¶ Returns or sets the delta toe of wheel.
It is used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Relative
.-------------------------------------
Getter Method
Signature
DeltaToe()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeltaToe(deltaToe)
Parameters: deltaToe (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DeltaX¶
-
BaseDataLoadingWheelBuilder.
DeltaX
¶ Returns or sets the delta x value of wheel center point.
It is used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Relative
.-------------------------------------
Getter Method
Signature
DeltaX()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeltaX(deltaX)
Parameters: deltaX (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DeltaY¶
-
BaseDataLoadingWheelBuilder.
DeltaY
¶ Returns or sets the delta y value of wheel center point.
It is used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Relative
.-------------------------------------
Getter Method
Signature
DeltaY()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeltaY(deltaY)
Parameters: deltaY (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DeltaZ¶
-
BaseDataLoadingWheelBuilder.
DeltaZ
¶ Returns or sets the delta z value of wheel center point.
It is used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Relative
.-------------------------------------
Getter Method
Signature
DeltaZ()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeltaZ(deltaZ)
Parameters: deltaZ (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DesignData¶
-
BaseDataLoadingWheelBuilder.
DesignData
¶ Returns or sets the design data of the wheel.
-------------------------------------
Getter Method
Signature
DesignData()
Returns: Return type: NXOpen.Features.VehicleDesign.BaseDataWheelBuilder
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignData(wheel)
Parameters: wheel ( NXOpen.Features.VehicleDesign.BaseDataWheelBuilder
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
StaticRadius¶
-
BaseDataLoadingWheelBuilder.
StaticRadius
¶ Returns or sets the static radius of wheel.
Used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Absolute
.-------------------------------------
Getter Method
Signature
StaticRadius()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StaticRadius(staticRadius)
Parameters: staticRadius (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Toe¶
-
BaseDataLoadingWheelBuilder.
Toe
¶ Returns or sets the toe in/out of wheel in degree.
Used only when
NXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilder.DataDefinition
isNXOpen.Features.VehicleDesign.BaseDataLoadingWheelBuilderDataDefinitionOptions.Absolute
.-------------------------------------
Getter Method
Signature
Toe()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Toe(toe)
Parameters: toe (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
BaseDataLoadingWheelBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.