BaseDataDriverBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
BaseDataDriverBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.VehicleDesign.BaseDataDriverBuilder
.This class can only be used in base data, thus cannot be created directly by user.
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
BackAngle | Returns the inclination angle of the backrest. |
BackAngleFixed | Returns or sets the option to indicate whether the Back Angle is fixed for not. |
DriverSide | Returns the Driver side. |
FrontShoulderRoom | Returns the front shoulder room. |
HeelReferencePoint | Returns or sets the driver heel reference point. |
HeelReferencePointActive | Returns or sets the status to indicate whether the driver heel reference point is active or not. |
HorizontalPointTravel | Returns the horizontal seat adjustment in the direction of the x axis. |
PedalReferencePoint | Returns or sets the driver pedal reference point. |
PedalReferencePointActive | Returns or sets the driver pedal reference point’s activeness. |
RearShoulderRoom | Returns the rear shoulder room. |
SeatReferencePoint | Returns or sets the driver seat reference point. |
SeatReferencePointActive | Returns or sets the status to indicate whether the driver seat reference point is active or not. |
SteeringWheelCenterPoint | Returns or sets the center point of the driver steering wheel. |
SteeringWheelCenterPointActive | Returns or sets the status to indicate whether the steering wheel center point is active or not. |
Tag | Returns the Tag for this object. |
Transmission | Returns or sets the vehicle transmission type. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BackAngle¶
-
BaseDataDriverBuilder.
BackAngle
¶ Returns the inclination angle of the backrest.
-------------------------------------
Getter Method
Signature
BackAngle()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
BackAngleFixed¶
-
BaseDataDriverBuilder.
BackAngleFixed
¶ Returns or sets the option to indicate whether the Back Angle is fixed for not.
If it is true, the back angle is not adjustable.
-------------------------------------
Getter Method
Signature
BackAngleFixed()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BackAngleFixed(driverBackAngleFixed)
Parameters: driverBackAngleFixed (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DriverSide¶
-
BaseDataDriverBuilder.
DriverSide
¶ Returns the Driver side.
This value indicates either it is a left driven or right driven vehicle. This value is calculated from the driver’s seat reference point coordinates and can not be edited by the user.
-------------------------------------
Getter Method
Signature
DriverSide()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
FrontShoulderRoom¶
-
BaseDataDriverBuilder.
FrontShoulderRoom
¶ Returns the front shoulder room.
This information is needed in the calculation for eye ellipses and the head position contour.
-------------------------------------
Getter Method
Signature
FrontShoulderRoom()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
HeelReferencePoint¶
-
BaseDataDriverBuilder.
HeelReferencePoint
¶ Returns or sets the driver heel reference point.
-------------------------------------
Getter Method
Signature
HeelReferencePoint()
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeelReferencePoint(refPoint)
Parameters: refPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
HeelReferencePointActive¶
-
BaseDataDriverBuilder.
HeelReferencePointActive
¶ Returns or sets the status to indicate whether the driver heel reference point is active or not.
If it is true, the driver heel reference point is active.
-------------------------------------
Getter Method
Signature
HeelReferencePointActive()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeelReferencePointActive(activeStatus)
Parameters: activeStatus (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
HorizontalPointTravel¶
-
BaseDataDriverBuilder.
HorizontalPointTravel
¶ Returns the horizontal seat adjustment in the direction of the x axis.
-------------------------------------
Getter Method
Signature
HorizontalPointTravel()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
PedalReferencePoint¶
-
BaseDataDriverBuilder.
PedalReferencePoint
¶ Returns or sets the driver pedal reference point.
-------------------------------------
Getter Method
Signature
PedalReferencePoint()
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PedalReferencePoint(refPoint)
Parameters: refPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PedalReferencePointActive¶
-
BaseDataDriverBuilder.
PedalReferencePointActive
¶ Returns or sets the driver pedal reference point’s activeness.
If true, the driver pedal reference point is active.
-------------------------------------
Getter Method
Signature
PedalReferencePointActive()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PedalReferencePointActive(activeStatus)
Parameters: activeStatus (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearShoulderRoom¶
-
BaseDataDriverBuilder.
RearShoulderRoom
¶ Returns the rear shoulder room.
This information is needed in the calculation for head position contour.
-------------------------------------
Getter Method
Signature
RearShoulderRoom()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
SeatReferencePoint¶
-
BaseDataDriverBuilder.
SeatReferencePoint
¶ Returns or sets the driver seat reference point.
-------------------------------------
Getter Method
Signature
SeatReferencePoint()
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeatReferencePoint(refPoint)
Parameters: refPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SeatReferencePointActive¶
-
BaseDataDriverBuilder.
SeatReferencePointActive
¶ Returns or sets the status to indicate whether the driver seat reference point is active or not.
If it is true, the driver seat reference point is active.
-------------------------------------
Getter Method
Signature
SeatReferencePointActive()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeatReferencePointActive(activeStatus)
Parameters: activeStatus (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SteeringWheelCenterPoint¶
-
BaseDataDriverBuilder.
SteeringWheelCenterPoint
¶ Returns or sets the center point of the driver steering wheel.
-------------------------------------
Getter Method
Signature
SteeringWheelCenterPoint()
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SteeringWheelCenterPoint(refPoint)
Parameters: refPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SteeringWheelCenterPointActive¶
-
BaseDataDriverBuilder.
SteeringWheelCenterPointActive
¶ Returns or sets the status to indicate whether the steering wheel center point is active or not.
If it is true, the steering wheel center point is active.
-------------------------------------
Getter Method
Signature
SteeringWheelCenterPointActive()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SteeringWheelCenterPointActive(activeStatus)
Parameters: activeStatus (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Transmission¶
-
BaseDataDriverBuilder.
Transmission
¶ Returns or sets the vehicle transmission type.
-------------------------------------
Getter Method
Signature
Transmission()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Transmission(transmission)
Parameters: transmission (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
BaseDataDriverBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.