UserDefinedFeatureIconEvent Class¶
-
class
NXOpen.Features.
UserDefinedFeatureIconEvent
¶ Bases:
NXOpen.TaggedObject
JA interface for the UserDefinedFeatureIconEvent object
This calls cannot be created
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ClassName | Returns the class name |
IconName | Returns or sets the icon name |
Instantiation | Returns the UDF instantiation feature |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
ClassName¶
-
UserDefinedFeatureIconEvent.
ClassName
¶ Returns the class name
-------------------------------------
Getter Method
Signature
ClassName()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
IconName¶
-
UserDefinedFeatureIconEvent.
IconName
¶ Returns or sets the icon name
-------------------------------------
Getter Method
Signature
IconName()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IconName(className)
Parameters: className (str) – New in version NX8.0.0.
License requirements: None.
Instantiation¶
-
UserDefinedFeatureIconEvent.
Instantiation
¶ Returns the UDF instantiation feature
-------------------------------------
Getter Method
Signature
Instantiation()
Returns: The UDF instantiation feature Return type: NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: None.