UserDefinedFeatureEditEvent Class¶
-
class
NXOpen.Features.
UserDefinedFeatureEditEvent
¶ Bases:
NXOpen.TaggedObject
JA interface for the UserDefinedFeatureEditEvent object
This calls cannot be created
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ClassName | Returns the class name |
Feature | Returns the related UDF |
Response | Returns or sets the response |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
ClassName¶
-
UserDefinedFeatureEditEvent.
ClassName
¶ Returns the class name
-------------------------------------
Getter Method
Signature
ClassName()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
Feature¶
-
UserDefinedFeatureEditEvent.
Feature
¶ Returns the related UDF
-------------------------------------
Getter Method
Signature
Feature()
Returns: The UDF that caused the event to fire Return type: NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: None.
Response¶
-
UserDefinedFeatureEditEvent.
Response
¶ Returns or sets the response
-------------------------------------
Getter Method
Signature
Response()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Response(response)
Parameters: response (int) – New in version NX8.0.0.
License requirements: None.