TrimCurveBuilderFirstBoundingObjectEndOptions Enumeration¶
NXOpen.Features.TrimCurveBuilder.FirstBoundingObjectEndOptions is an alias for NXOpen.Features.TrimCurveBuilderFirstBoundingObjectEndOptions
-
class
NXOpen.Features.
TrimCurveBuilderFirstBoundingObjectEndOptions
¶ Bases:
object
Represents the trim curve first bounding object end options
Enum Members
Enum Member Enum Member Description Start Trim first bounding object from startEnd Trim first bounding object from end-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-