ThroughCurveMeshBuilderEmphasisType Enumeration¶
NXOpen.Features.ThroughCurveMeshBuilder.EmphasisType is an alias for NXOpen.Features.ThroughCurveMeshBuilderEmphasisType
-
class
NXOpen.Features.
ThroughCurveMeshBuilderEmphasisType
¶ Bases:
object
This enum represents the Emphasis options.
Enum Members
Enum Member Enum Member Description Both Emphasis on both primary and cross strings.Primary Emphasis on primary strings.Cross Emphasis on cross strings.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-