TabNoteCfgBuilderRefplane Enumeration¶
NXOpen.Features.TabNoteCfgBuilder.Refplane is an alias for NXOpen.Features.TabNoteCfgBuilderRefplane
-
class
NXOpen.Features.
TabNoteCfgBuilderRefplane
¶ Bases:
object
the reference plane type.
Enum Members
Enum Member Enum Member Description Xy 0 : Xc-Yc planeYz 1 : Yc-Zc planeZx 2 : Zc-Xc planeNegXy 3 : - Xc-Yc planeNegYz 4 : - Yc-Zc planeNegZx 5 : - Zc-Xc plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-