SweptBuilderInterpolationOptions Enumeration¶
NXOpen.Features.SweptBuilder.InterpolationOptions is an alias for NXOpen.Features.SweptBuilderInterpolationOptions
-
class
NXOpen.Features.
SweptBuilderInterpolationOptions
¶ Bases:
object
This enum represents the Interpolation option.
For 2 or more sections, this option specifies the method by which to interpolate between them, either Linear or Cubic.
Enum Members
Enum Member Enum Member Description Linear LinearCubic CubicBlend Blend-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-