ExtractCagePolylineBuilder Class¶
-
class
NXOpen.Features.Subdivision.
ExtractCagePolylineBuilder
¶ Bases:
NXOpen.Builder
Extract cage polyline builder class.
To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateExtractCagePolylineBuilder
Default values.
Property Value NumberOfSegments 4 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
CurveToExtract | Returns the curve to extract |
InputCurveOptions | Returns or sets the input curve options |
NumberOfSegments | Returns or sets the number of segments |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExtractCagePolylineBuilderInputCurveOption Enumeration | Input curves options. |
Property Detail¶
CurveToExtract¶
-
ExtractCagePolylineBuilder.
CurveToExtract
¶ Returns the curve to extract
-------------------------------------
Getter Method
Signature
CurveToExtract()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
InputCurveOptions¶
-
ExtractCagePolylineBuilder.
InputCurveOptions
¶ Returns or sets the input curve options
-------------------------------------
Getter Method
Signature
InputCurveOptions()
Returns: Return type: NXOpen.Features.Subdivision.ExtractCagePolylineBuilderInputCurveOption
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InputCurveOptions(inputCurveOptions)
Parameters: inputCurveOptions ( NXOpen.Features.Subdivision.ExtractCagePolylineBuilderInputCurveOption
) –New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
NumberOfSegments¶
-
ExtractCagePolylineBuilder.
NumberOfSegments
¶ Returns or sets the number of segments
-------------------------------------
Getter Method
Signature
NumberOfSegments()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfSegments(numberOfSegments)
Parameters: numberOfSegments (int) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Method Detail¶
Validate¶
-
ExtractCagePolylineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.