CageManipulatorDataObjectSelectionData_Struct Struct¶
NXOpen.Features.Subdivision.CageManipulatorData.ObjectSelectionData is an alias for NXOpen.Features.Subdivision.CageManipulatorDataObjectSelectionData_Struct
-
class
NXOpen.Features.Subdivision.
CageManipulatorDataObjectSelectionData_Struct
¶ Bases:
object
Contains object selection information.
New in version NX9.0.0.
Fields¶
Field | Description |
---|---|
SelectedObject | The selected object. |
SelectionPosition | The point at which object is selected, the point under the cursor when seen in view direction. |
ViewDirection | The view direction. |
IsSnappedPosition | Is SelectionPosition a snapped location. |
SelectedObject¶
-
CageManipulatorDataObjectSelectionData_Struct.
SelectedObject
¶ The selected object.
-------------------------------------
Getter Method Signature
SelectedObject()
Returns: Return type: NXOpen.NXObject
-------------------------------------
Setter Method
Signature
SelectedObject(value)
Parameters: value ( NXOpen.NXObject
) –
SelectionPosition¶
-
CageManipulatorDataObjectSelectionData_Struct.
SelectionPosition
¶ The point at which object is selected, the point under the cursor when seen in view direction.
-------------------------------------
Getter Method Signature
SelectionPosition()
Returns: Return type: NXOpen.Point3d
-------------------------------------
Setter Method
Signature
SelectionPosition(value)
Parameters: value ( NXOpen.Point3d
) –
ViewDirection¶
-
CageManipulatorDataObjectSelectionData_Struct.
ViewDirection
¶ The view direction.
-------------------------------------
Getter Method Signature
ViewDirection()
Returns: Return type: NXOpen.Vector3d
-------------------------------------
Setter Method
Signature
ViewDirection(value)
Parameters: value ( NXOpen.Vector3d
) –
IsSnappedPosition¶
-
CageManipulatorDataObjectSelectionData_Struct.
IsSnappedPosition
¶ Is SelectionPosition a snapped location.
-------------------------------------
Getter Method Signature
IsSnappedPosition()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
IsSnappedPosition(value)
Parameters: value (bool) –