StudioXformBuilderTypes Enumeration¶
NXOpen.Features.StudioXformBuilder.Types is an alias for NXOpen.Features.StudioXformBuilderTypes
-
class
NXOpen.Features.
StudioXformBuilderTypes
¶ Bases:
object
Represents the Xform type
Enum Members
Enum Member Enum Member Description Translate Translate type of XformRotate Rotate type of XformScale Scale type of XformTranslateNormalToFaceOrCurve Along normal type of XformTranlsateAlongControlPolygon Along polygon type of XformPlanarizeRowOfPoles Planarize type of Xform-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-