StudioXformBuilderTranslationDirectionType Enumeration¶
NXOpen.Features.StudioXformBuilder.TranslationDirectionType is an alias for NXOpen.Features.StudioXformBuilderTranslationDirectionType
-
class
NXOpen.Features.
StudioXformBuilderTranslationDirectionType
¶ Bases:
object
Represents the translation direction type
Enum Members
Enum Member Enum Member Description Xc Translate in X directionYc Translate in Y directionZc Translate in Z directionYcZc Translate on Y-Z planeXcZc Translate on X-Z planeXcYc Translate on X-Y planeArbitraryDirection Translate in arbitrary directionArbitraryPlane Translate on arbitrary plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-