StudioXformBuilderPlanarizeMethodType Enumeration¶
NXOpen.Features.StudioXformBuilder.PlanarizeMethodType is an alias for NXOpen.Features.StudioXformBuilderPlanarizeMethodType
-
class
NXOpen.Features.
StudioXformBuilderPlanarizeMethodType
¶ Bases:
object
Represents the planarize method type
Enum Members
Enum Member Enum Member Description AtPlaneLocation planarize at plane locationAtPoleLocation planarize at pole locationOnABestFitPlane planarize at a best fit plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-