StudioXformBuilderAdvancedMethodType Enumeration¶
NXOpen.Features.StudioXformBuilder.AdvancedMethodType is an alias for NXOpen.Features.StudioXformBuilderAdvancedMethodType
-
class
NXOpen.Features.
StudioXformBuilderAdvancedMethodType
¶ Bases:
object
Represents the advanced method type
Enum Members
Enum Member Enum Member Description ChangeDegree Change degreeFalloff Fall offProportionalMovement Proportional movementKeepContinuity Keep continuityLockRegion Lock regionInsertKnot Insert knotAdvanceOff Turn off advanced methods-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-