StudioSurfaceBuilderTransitionOptions Enumeration¶
NXOpen.Features.StudioSurfaceBuilder.TransitionOptions is an alias for NXOpen.Features.StudioSurfaceBuilderTransitionOptions
-
class
NXOpen.Features.
StudioSurfaceBuilderTransitionOptions
¶ Bases:
object
the transition control options when using By Points alignment method
Enum Members
Enum Member Enum Member Description NormalToEndSections Normal to End SectionsNormalToAllSections Normal to All SectionsCubic CubicLinearAndBlend Linear and BlendNoEndConstraint No End Constraint-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-