StudioSplineBuilderCurveOption Enumeration¶
NXOpen.Features.StudioSplineBuilder.CurveOption is an alias for NXOpen.Features.StudioSplineBuilderCurveOption
-
class
NXOpen.Features.
StudioSplineBuilderCurveOption
¶ Bases:
object
Options of the actions to be taken on an input non-parametric spline after its editing is done.
These options are used only while trying to make non-parametric spline a feature.
Enum Members
Enum Member Enum Member Description Retain Retain input curveBlank Blank input curveDelete Delete input curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-