StepBuilderStepWallMethods Enumeration¶
NXOpen.Features.StepBuilder.StepWallMethods is an alias for NXOpen.Features.StepBuilderStepWallMethods
-
class
NXOpen.Features.
StepBuilderStepWallMethods
¶ Bases:
object
Represents face operation applied to the step wall face
Enum Members
Enum Member Enum Member Description Normal Orients the step-wall face normal to the input face OffsetofStepFace Makes the step-wall face offset from the step face ExtendtoNext Extends the wall face to intersect the next face -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-