StepBuilderReferenceBoundaryTypes Enumeration¶
NXOpen.Features.StepBuilder.ReferenceBoundaryTypes is an alias for NXOpen.Features.StepBuilderReferenceBoundaryTypes
-
class
NXOpen.Features.
StepBuilderReferenceBoundaryTypes
¶ Bases:
object
Represents selected type as reference boundary object
Enum Members
Enum Member Enum Member Description Face Select faces as reference boundary objectDatumPlane Select datum plane as reference boundary objectCurve Select section curves as reference boundary objectEdge Select edges as reference boundary object-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-