SmoothRangeBuilder Class¶
-
class
NXOpen.Features.
SmoothRangeBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.SmoothRangeBuilder
builderTo create a new instance of this class, use
NXOpen.Features.FlowBlendBuilder.NewSmoothRange
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
SmoothRangeFrom | Returns or sets the start point of smoothing range |
SmoothRangeTo | Returns or sets the end point of smoothing range |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SmoothRangeFrom¶
-
SmoothRangeBuilder.
SmoothRangeFrom
¶ Returns or sets the start point of smoothing range
-------------------------------------
Getter Method
Signature
SmoothRangeFrom()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothRangeFrom(smoothRangeFrom)
Parameters: smoothRangeFrom ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SmoothRangeTo¶
-
SmoothRangeBuilder.
SmoothRangeTo
¶ Returns or sets the end point of smoothing range
-------------------------------------
Getter Method
Signature
SmoothRangeTo()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothRangeTo(smoothRangeTo)
Parameters: smoothRangeTo ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
SmoothRangeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.