SmoothCurveStringBuilderMergeTypes Enumeration¶
NXOpen.Features.SmoothCurveStringBuilder.MergeTypes is an alias for NXOpen.Features.SmoothCurveStringBuilderMergeTypes
-
class
NXOpen.Features.
SmoothCurveStringBuilderMergeTypes
¶ Bases:
object
the options to merge curves after being made continuous.
Enum Members
Enum Member Enum Member Description None no merging of curvesSameTypes merge only spline curvesAllCurves merge all types of curves-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-