SectionSurfaceBuilderTypes Enumeration¶
NXOpen.Features.SectionSurfaceBuilder.Types is an alias for NXOpen.Features.SectionSurfaceBuilderTypes
-
class
NXOpen.Features.
SectionSurfaceBuilderTypes
¶ Bases:
object
This enum represents the current types of section surface methods
Enum Members
Enum Member Enum Member Description EndsApexShoulder ends apex shoulderEndsSlopeShoulder ends slope shoulderFilletShoulder fillet shoulderEndsApexRho ends apex rhoEndsSlopeRho ends slope rhoFilletRho fillet rhoEndsApexHilite ends apex hiliteEndsSlopeHilite ends slope hiliteFilletHilite fillet hiliteFourPointSlope four point slopeFivePoint five pointThreePointArc three point arcTwoPointRadius two point radiusEndSlopeArc point radius angle arcPointRadiusAngleArc point radius angle arcCircle circleCircleTangent circle tangentEndsSlopeCubic ends slope cubicFilletBridge fillet bridgeLinearTangent linear tangent-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-