SectionSurfaceBuilderControlRegionEnum Enumeration¶
NXOpen.Features.SectionSurfaceBuilder.ControlRegionEnum is an alias for NXOpen.Features.SectionSurfaceBuilderControlRegionEnum
-
class
NXOpen.Features.
SectionSurfaceBuilderControlRegionEnum
¶ Bases:
object
This enum represents the type of the region where depth and skew can be applied
Enum Members
Enum Member Enum Member Description Entire depth and skew applied to the entire section surfaceStart depth and skew applied to the start section of the section surfaceEnd depth and skew applied to the end section of the section surface-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-