ReplaceFaceBuilderReplaceTypes Enumeration¶
NXOpen.Features.ReplaceFaceBuilder.ReplaceTypes is an alias for NXOpen.Features.ReplaceFaceBuilderReplaceTypes
-
class
NXOpen.Features.
ReplaceFaceBuilderReplaceTypes
¶ Bases:
object
Enumeration of replace face type, don’t use it until nx502
New in version NX5.0.2.
Enum Members
Enum Member Enum Member Description Replace This stands for replace type - to replace the surface of the target face with the tool faceSimplify This stands for simplify type - to simplify the geometry representation of a surface of a face-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-