PolylineBuilderWCSOptionType Enumeration¶
NXOpen.Features.PolylineBuilder.WCSOptionType is an alias for NXOpen.Features.PolylineBuilderWCSOptionType
-
class
NXOpen.Features.
PolylineBuilderWCSOptionType
¶ Bases:
object
WCS principal axis or plane types
Enum Members
Enum Member Enum Member Description X Along X axisY Along Y axisZ Along Z axisYZ In YZ planeXZ In XZ planeXY In XY plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-