PointSetBuilderCurvePointsType Enumeration¶
NXOpen.Features.PointSetBuilder.CurvePointsType is an alias for NXOpen.Features.PointSetBuilderCurvePointsType
-
class
NXOpen.Features.
PointSetBuilderCurvePointsType
¶ Bases:
object
The settings for the curve points definition.
Enum Members
Enum Member Enum Member Description EqualArcLength Points will be created at equal arc length along curve.EqualParameters Points will be created at equal parameter spacing along curve.GeometricProgression Points will be created with a geometric progression along curve.ChordalTolerance Points will be created based on the chordal deviation of curve.IncrementalArcLength A point will be created at the arc length spacing input.SpecifiedProjectionPoints Points will be created at minimum distance to curve.CurvePercentage A point will be created at given curve percentage.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-