PatternFaceBuilderPatternTypes Enumeration¶
NXOpen.Features.PatternFaceBuilder.PatternTypes is an alias for NXOpen.Features.PatternFaceBuilderPatternTypes
-
class
NXOpen.Features.
PatternFaceBuilderPatternTypes
¶ Bases:
object
Enumeration of pattern type, don’t use it until nx502
New in version NX5.0.2.
Enum Members
Enum Member Enum Member Description Rectangular This stands for rectangular pattern type.Circular This stands for circular pattern type.Mirror This stands for mirror pattern type.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-