PatchOpeningsBuilderTypes Enumeration¶
NXOpen.Features.PatchOpeningsBuilder.Types is an alias for NXOpen.Features.PatchOpeningsBuilderTypes
-
class
NXOpen.Features.
PatchOpeningsBuilderTypes
¶ Bases:
object
The method used to patch the opening
Enum Members
Enum Member Enum Member Description Quilted Patch with quilted patchwork of facesNSided Patch with N-sided surface area methodMesh Patch with through curve meshByDeletingEdges Patch by deleting edges and growing facesExtension Tangent edge extension methodNotch Notch fill methodJoggle Joggle fill methodMoldWizard Patch with Mold wizard edge patch methodBySuppression Patch by suppressing features-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-