PartModulePartLoadOption Enumeration¶
NXOpen.Features.PartModule.PartLoadOption is an alias for NXOpen.Features.PartModulePartLoadOption
-
class
NXOpen.Features.
PartModulePartLoadOption
¶ Bases:
object
Defines part load options
Enum Members
Enum Member Enum Member Description DontAllowSave Sets the loaded part as read only. Allow changes in the part, but part cannot be savedLoadInterpart If this option is set, First it will check part is modified or not, then loads interpart of Part Module otherwise reload the own part of Part Module-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-