OvercrownBuilderOutputType Enumeration¶
NXOpen.Features.OvercrownBuilder.OutputType is an alias for NXOpen.Features.OvercrownBuilderOutputType
-
class
NXOpen.Features.
OvercrownBuilderOutputType
¶ Bases:
object
This enum represents the output type of Global Shaping Operation
Enum Members
Enum Member Enum Member Description Sheet Solid -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-