MoveObjectBuilderLayerOptionType Enumeration¶
NXOpen.Features.MoveObjectBuilder.LayerOptionType is an alias for NXOpen.Features.MoveObjectBuilderLayerOptionType
-
class
NXOpen.Features.
MoveObjectBuilderLayerOptionType
¶ Bases:
object
Indicates the layer on which moved or copied objects will be placed
Enum Members
Enum Member Enum Member Description Original Original LayerWork Work LayerAsSpecified As Specified Layer-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-