MidSurfaceByFacePairsBuilderTrimmingOptionType Enumeration¶
NXOpen.Features.MidSurfaceByFacePairsBuilder.TrimmingOptionType is an alias for NXOpen.Features.MidSurfaceByFacePairsBuilderTrimmingOptionType
-
class
NXOpen.Features.
MidSurfaceByFacePairsBuilderTrimmingOptionType
¶ Bases:
object
trimming options
Enum Members
Enum Member Enum Member Description AdvancedTrimming Advanced trimming BodyBasedTrimming Body based trimming TrimtoSide1withNoExtension Trim to master SkipTrimming Skip trimming for replacement sheets -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-