MidSurfaceByFacePairsBuilderSurfaceType Enumeration¶
NXOpen.Features.MidSurfaceByFacePairsBuilder.SurfaceType is an alias for NXOpen.Features.MidSurfaceByFacePairsBuilderSurfaceType
-
class
NXOpen.Features.
MidSurfaceByFacePairsBuilderSurfaceType
¶ Bases:
object
midsurface options
Enum Members
Enum Member Enum Member Description Standard Default surface creation method Side1 Use side 1 faces as mid sheet Offset Use offset CloudOfPoints Cloud of points Large Use single largest surface -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-