MatchedReferenceBuilderTypes Enumeration¶
NXOpen.Features.MatchedReferenceBuilder.Types is an alias for NXOpen.Features.MatchedReferenceBuilderTypes
-
class
NXOpen.Features.
MatchedReferenceBuilderTypes
¶ Bases:
object
MatchedReference block type
Enum Members
Enum Member Enum Member Description Curve single curve or edgeFace single face or datum planeCurveCollector curve collector or edge collectorFaceCollector face collectorSection sectionPoint pointVector vectorObject general geometry such as the target body and the tool body for copying unite featureBodyCollector body collectorCsys csysPlane planeAxis axisUndefined default type for feature name lable-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-