MatchEdgeBuilderPoleMovementConstraintEnumType Enumeration¶
NXOpen.Features.MatchEdgeBuilder.PoleMovementConstraintEnumType is an alias for NXOpen.Features.MatchEdgeBuilderPoleMovementConstraintEnumType
-
class
NXOpen.Features.
MatchEdgeBuilderPoleMovementConstraintEnumType
¶ Bases:
object
Pole movement type
Enum Members
Enum Member Enum Member Description WCS Along WCS X/Y/Z directionView Along viewVector Along user defined vectorNormal NormalProject ProjectInherit InheritFixStart Fix startFixEnd Fix endStartAndEnd Fix start and end-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-