LawExtensionBuilderExMiterOptions Enumeration¶
NXOpen.Features.LawExtensionBuilderEx.MiterOptions is an alias for NXOpen.Features.LawExtensionBuilderExMiterOptions
-
class
NXOpen.Features.
LawExtensionBuilderExMiterOptions
¶ Bases:
object
Miter options
Enum Members
Enum Member Enum Member Description None No miter solution between two discontinuous facesSharp Creates a sharp edge between two facesBlend Creates a three-sided patch between two facesRadius Creates a four-sided patch between two faces-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-