JoeBuilderDiscreetTypes Enumeration¶
NXOpen.Features.JoeBuilder.DiscreetTypes is an alias for NXOpen.Features.JoeBuilderDiscreetTypes
-
class
NXOpen.Features.
JoeBuilderDiscreetTypes
¶ Bases:
object
Enumeration of discreet types
New in version NX5.0.0.
Enum Members
Enum Member Enum Member Description Option1 Option2 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-