HolePackageBuilderThreadLengthOptions Enumeration¶
NXOpen.Features.HolePackageBuilder.ThreadLengthOptions is an alias for NXOpen.Features.HolePackageBuilderThreadLengthOptions
-
class
NXOpen.Features.
HolePackageBuilderThreadLengthOptions
¶ Bases:
object
Represents thread length options.
This option is applicable for the threaded hole.
Enum Members
Enum Member Enum Member Description Diameterx1 1 * (tap drill diameter)Diameterx15 1.5 * (tap drill diameter)Diameterx20 2 * (tap drill diameter)Diameterx25 2.5 * (tap drill diameter)Diameterx30 3 * (tap drill diameter)Standard Length is StandardCustom Length is customFull Length is full hole depth-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-