HelixBuilderOrientationOptions Enumeration¶
NXOpen.Features.HelixBuilder.OrientationOptions is an alias for NXOpen.Features.HelixBuilderOrientationOptions
-
class
NXOpen.Features.
HelixBuilderOrientationOptions
¶ Bases:
object
Orientation options for along spine type
Enum Members
Enum Member Enum Member Description Inferred Local coordinate system is inferred from spine, at the startSpecified Local coordinate system is specified by the user. The spine is transformed using this coordinate system.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-