GlobalShapingBuilderDirectionMethodType Enumeration¶
NXOpen.Features.GlobalShapingBuilder.DirectionMethodType is an alias for NXOpen.Features.GlobalShapingBuilderDirectionMethodType
-
class
NXOpen.Features.
GlobalShapingBuilderDirectionMethodType
¶ Bases:
object
Represents the direction method type.
Enum Members
Enum Member Enum Member Description SameAsProjection Overcrown is same as projection directionNormalToSheet Overcrown is normal to sheetNormalToBase Overcrown is normal to base surfaceNormalToControl Overcrown is normal to control surfaceSpecifiedDirection Overcrown is user specified directionNone Overcrown has no direction specified-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-