GeometricConstraintDataSetManager Class¶
-
class
NXOpen.Features.
GeometricConstraintDataSetManager
¶ Bases:
NXOpen.TaggedObject
Represents Geometric Constraint Data Set Manager class.
This class maintains a list of
NXOpen.Features.GeometricConstraintDataManager
objects and manages them.New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Length | Returns the number of manager objects in the list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Append | Appends NXOpen.Features.GeometricConstraintDataManager object to the end of the list |
CreateGeometricConstraintDataManager | Creates a new empty NXOpen.Features.GeometricConstraintDataManager object @return |
Delete | Deletes NXOpen.Features.GeometricConstraintDataManager object from the list |
GetContents | Queries all the manager objects @return |
GetIndex | Finds index of NXOpen.Features.GeometricConstraintDataManager in the list. |
Insert | Inserts NXOpen.Features.GeometricConstraintDataManager object in the list before a given position |
SetContents | Sets array of manager objects in the list. |
Property Detail¶
Method Detail¶
Append¶
-
GeometricConstraintDataSetManager.
Append
¶ Appends
NXOpen.Features.GeometricConstraintDataManager
object to the end of the listSignature
Append(manager)
Parameters: manager ( NXOpen.Features.GeometricConstraintDataManager
) –New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”)
CreateGeometricConstraintDataManager¶
-
GeometricConstraintDataSetManager.
CreateGeometricConstraintDataManager
¶ Creates a new empty
NXOpen.Features.GeometricConstraintDataManager
objectSignature
CreateGeometricConstraintDataManager()
Returns: Return type: NXOpen.Features.GeometricConstraintDataManager
New in version NX5.0.0.
License requirements: None.
Delete¶
-
GeometricConstraintDataSetManager.
Delete
¶ Overloaded method Delete
Delete(manager)
Delete(managerIndex)
-------------------------------------
Deletes
NXOpen.Features.GeometricConstraintDataManager
object from the listSignature
Delete(manager)
Parameters: manager ( NXOpen.Features.GeometricConstraintDataManager
) –New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”)
-------------------------------------
Deletes Nth
NXOpen.Features.GeometricConstraintDataManager
object from the listSignature
Delete(managerIndex)
Parameters: managerIndex (int) – New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”)
-------------------------------------
GetContents¶
-
GeometricConstraintDataSetManager.
GetContents
¶ Queries all the manager objects
Signature
GetContents()
Returns: Return type: list of NXOpen.Features.GeometricConstraintDataManager
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetIndex¶
-
GeometricConstraintDataSetManager.
GetIndex
¶ Finds index of
NXOpen.Features.GeometricConstraintDataManager
in the list.Returns -1 if not found
Signature
GetIndex(manager)
Parameters: manager ( NXOpen.Features.GeometricConstraintDataManager
) –Returns: Return type: int New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Insert¶
-
GeometricConstraintDataSetManager.
Insert
¶ Inserts
NXOpen.Features.GeometricConstraintDataManager
object in the list before a given positionSignature
Insert(insertBeforeIndex, manager)
Parameters: - insertBeforeIndex (int) –
- manager (
NXOpen.Features.GeometricConstraintDataManager
) –
New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”)
SetContents¶
-
GeometricConstraintDataSetManager.
SetContents
¶ Sets array of manager objects in the list.
Before setting new array of objects, deletes all the previous objects in the list.
Signature
SetContents(managers)
Parameters: managers (list of NXOpen.Features.GeometricConstraintDataManager
) –New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”)