GeometricConstraintDataParameterDirection Enumeration¶
NXOpen.Features.GeometricConstraintData.ParameterDirection is an alias for NXOpen.Features.GeometricConstraintDataParameterDirection
-
class
NXOpen.Features.
GeometricConstraintDataParameterDirection
¶ Bases:
object
Parameter direction to be used for creation of the constraint at a point which is attached to an object, for example a curve or a face
Enum Members
Enum Member Enum Member Description Iso Iso parameterSection General section if point is attached to faceNormal NormalPerpendicular Perpendicular to curve on face or edge-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-