GeodesicTrimBuilder Class¶
-
class
NXOpen.Features.
GeodesicTrimBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.GeodesicSketch
builder for GeodesicTrim command.To create a new instance of this class, use
NXOpen.Features.GeodesicSketchCollection.CreateGeodesicTrimBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Curve | Returns or sets the curve to trim |
ExtentCurve | Returns or sets the extent curve defines the region to be removed from the curve |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Point | Returns or sets the selection point |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Curve¶
-
GeodesicTrimBuilder.
Curve
¶ Returns or sets the curve to trim
-------------------------------------
Getter Method
Signature
Curve()
Returns: NXOpen.Curve
Return type: NXOpen.Curve
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Curve(curve)
Parameters: curve ( NXOpen.Curve
) –NXOpen.Curve
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ExtentCurve¶
-
GeodesicTrimBuilder.
ExtentCurve
¶ Returns or sets the extent curve defines the region to be removed from the curve
-------------------------------------
Getter Method
Signature
ExtentCurve()
Returns: Curve
Return type: NXOpen.Curve
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtentCurve(curve)
Parameters: curve ( NXOpen.Curve
) –Curve
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Point¶
-
GeodesicTrimBuilder.
Point
¶ Returns or sets the selection point
-------------------------------------
Getter Method
Signature
Point()
Returns: Point Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point (float) – Point New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
GeodesicTrimBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.