GeodesicIntersectBuilder Class¶
-
class
NXOpen.Features.
GeodesicIntersectBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.GeodesicIntersect
builder for Intersect command.To create a new instance of this class, use
NXOpen.Features.GeodesicSketchCollection.CreateGeodesicIntersectBuilder
Default values.
Property Value IntersectType Datum New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
IntersectCurves | Returns the curves to intersect sketch face |
IntersectDatum | Returns the datum plane or datum axis to intersect sketch face |
IntersectFaces | Returns the faces to intersect sketch face |
IntersectType | Returns or sets the intersect type |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GeodesicIntersectBuilderType Enumeration | Represents the type of objects that intersect with the support faces. |
Property Detail¶
IntersectCurves¶
-
GeodesicIntersectBuilder.
IntersectCurves
¶ Returns the curves to intersect sketch face
-------------------------------------
Getter Method
Signature
IntersectCurves()
Returns: Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
IntersectDatum¶
-
GeodesicIntersectBuilder.
IntersectDatum
¶ Returns the datum plane or datum axis to intersect sketch face
-------------------------------------
Getter Method
Signature
IntersectDatum()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX10.0.0.
License requirements: None.
IntersectFaces¶
-
GeodesicIntersectBuilder.
IntersectFaces
¶ Returns the faces to intersect sketch face
-------------------------------------
Getter Method
Signature
IntersectFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
IntersectType¶
-
GeodesicIntersectBuilder.
IntersectType
¶ Returns or sets the intersect type
-------------------------------------
Getter Method
Signature
IntersectType()
Returns: Return type: NXOpen.Features.GeodesicIntersectBuilderType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntersectType(intersectType)
Parameters: intersectType ( NXOpen.Features.GeodesicIntersectBuilderType
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
GeodesicIntersectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.