GeneralConicBuilderTypes Enumeration¶
NXOpen.Features.GeneralConicBuilder.Types is an alias for NXOpen.Features.GeneralConicBuilderTypes
-
class
NXOpen.Features.
GeneralConicBuilderTypes
¶ Bases:
object
General Conic Types.
There are several creation methods available. All except the
Types.Coefficients
type require setting points/slopes.Enum Members
Enum Member Enum Member Description FivePoints Five points, no slopes, no anchor, no rho valueFourPointsOneSlope Four points, one slope, no anchor, no rho valueThreePointsTwoSlopes Three points, two slopes, no anchor, no rho valueThreePointsAnchor Three points, no slopes, anchor, no rho valueTwoPointsAnchorRho Two points, no slopes, anchor, rho valueTwoPointsTwoSlopesRho Two points, two slopes, no anchor, rho valueCoefficients Coefficient values andCoefficientCSYS`
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-