GeneralConicBuilderDrawingPlaneOptions Enumeration¶
NXOpen.Features.GeneralConicBuilder.DrawingPlaneOptions is an alias for NXOpen.Features.GeneralConicBuilderDrawingPlaneOptions
-
class
NXOpen.Features.
GeneralConicBuilderDrawingPlaneOptions
¶ Bases:
object
Drawing Plane options.
Used by all point types to specify point selection guide planes.
Enum Members
Enum Member Enum Member Description View Use view planeXcYc Use XC-YC planeYcZc Use YC-ZC planeZcXc Use ZC-XC planeGeneral UseGeneralDrawingPlane`
plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-