FlatPatternObjectDataGeneral_Struct Struct¶
NXOpen.Features.FlatPattern.ObjectDataGeneral is an alias for NXOpen.Features.FlatPatternObjectDataGeneral_Struct
-
class
NXOpen.Features.
FlatPatternObjectDataGeneral_Struct
¶ Bases:
object
Structure used to return data about objects in the flat pattern.
This structure is for points whose associativities are not covered by the other types, which are returned as tagged objects. Used for the added geometry objects.
Fields¶
Field | Description |
---|---|
FlatPatternObject | Object in the flat pattern |
FlatSolidObject | Corresponding object on the flat solid |
FormedBodyObject | Corresponding object on the formed body |
FlatPatternObject¶
-
FlatPatternObjectDataGeneral_Struct.
FlatPatternObject
¶ Object in the flat pattern
-------------------------------------
Getter Method Signature
FlatPatternObject()
Returns: Return type: NXOpen.TaggedObject
-------------------------------------
Setter Method
Signature
FlatPatternObject(value)
Parameters: value ( NXOpen.TaggedObject
) –
FlatSolidObject¶
-
FlatPatternObjectDataGeneral_Struct.
FlatSolidObject
¶ Corresponding object on the flat solid
-------------------------------------
Getter Method Signature
FlatSolidObject()
Returns: Return type: NXOpen.TaggedObject
-------------------------------------
Setter Method
Signature
FlatSolidObject(value)
Parameters: value ( NXOpen.TaggedObject
) –
FormedBodyObject¶
-
FlatPatternObjectDataGeneral_Struct.
FormedBodyObject
¶ Corresponding object on the formed body
-------------------------------------
Getter Method Signature
FormedBodyObject()
Returns: Return type: NXOpen.TaggedObject
-------------------------------------
Setter Method
Signature
FormedBodyObject(value)
Parameters: value ( NXOpen.TaggedObject
) –