FlatPatternObjectDataFace_Struct Struct¶
NXOpen.Features.FlatPattern.ObjectDataFace is an alias for NXOpen.Features.FlatPatternObjectDataFace_Struct
-
class
NXOpen.Features.
FlatPatternObjectDataFace_Struct
¶ Bases:
object
Structure used to return data about objects in the flat pattern.
This structure is for curves whose associativities are faces.
Fields¶
Field | Description |
---|---|
FlatPatternObject | Curve in the flat pattern |
FlatSolidObject | Corresponding bend face on the flat solid |
FormedBodyObject | Corresponding bend face on the formed body |
FlatPatternObject¶
-
FlatPatternObjectDataFace_Struct.
FlatPatternObject
¶ Curve in the flat pattern
-------------------------------------
Getter Method Signature
FlatPatternObject()
Returns: Return type: NXOpen.Curve
-------------------------------------
Setter Method
Signature
FlatPatternObject(value)
Parameters: value ( NXOpen.Curve
) –
FlatSolidObject¶
-
FlatPatternObjectDataFace_Struct.
FlatSolidObject
¶ Corresponding bend face on the flat solid
-------------------------------------
Getter Method Signature
FlatSolidObject()
Returns: Return type: NXOpen.Face
-------------------------------------
Setter Method
Signature
FlatSolidObject(value)
Parameters: value ( NXOpen.Face
) –
FormedBodyObject¶
-
FlatPatternObjectDataFace_Struct.
FormedBodyObject
¶ Corresponding bend face on the formed body
-------------------------------------
Getter Method Signature
FormedBodyObject()
Returns: Return type: NXOpen.Face
-------------------------------------
Setter Method
Signature
FormedBodyObject(value)
Parameters: value ( NXOpen.Face
) –