FlatPatternObjectDataEdge_Struct Struct¶
NXOpen.Features.FlatPattern.ObjectDataEdge is an alias for NXOpen.Features.FlatPatternObjectDataEdge_Struct
-
class
NXOpen.Features.
FlatPatternObjectDataEdge_Struct
¶ Bases:
object
Structure used to return data about objects in the flat pattern.
This structure is for curves whose associativities are edges.
Fields¶
Field | Description |
---|---|
FlatPatternObject | Curve in the flat pattern |
FlatSolidObject | Corresponding edge on the flat solid |
FlatPatternObject¶
-
FlatPatternObjectDataEdge_Struct.
FlatPatternObject
¶ Curve in the flat pattern
-------------------------------------
Getter Method Signature
FlatPatternObject()
Returns: Return type: NXOpen.Curve
-------------------------------------
Setter Method
Signature
FlatPatternObject(value)
Parameters: value ( NXOpen.Curve
) –
FlatSolidObject¶
-
FlatPatternObjectDataEdge_Struct.
FlatSolidObject
¶ Corresponding edge on the flat solid
-------------------------------------
Getter Method Signature
FlatSolidObject()
Returns: Return type: NXOpen.Edge
-------------------------------------
Setter Method
Signature
FlatSolidObject(value)
Parameters: value ( NXOpen.Edge
) –